AnsweredAssumed Answered

S32 Design Studio for ARM 2018.R1 for Linux is shipped without SDK

Question asked by Maksim Salau on Apr 4, 2018
Latest reply on Apr 11, 2018 by Maksim Salau

Hello,

 

I've just installed the studio and can't find SDKs in it.

I.e. when I create a project for S32K144 I see the list on the attached screenshot:

 

The only SDK that is available for me is the one for S32K116 that was installed by the only update available.

Did something changed in the way SDKs are installed? I'm new to S32 and from tutorial I see that SDK should be ready out-of-the-box.

 

Thanks,

Maksim.

Outcomes