Hi All,
Trying to update FRDM-LS1012a reference board with prebuilt images.
Based on Getting started page of FRDM-LS1012a , Downloaded Image: QorIQ Linux SDK v2.0 AARCH64 IMAGE.
But that only contains LS1043ARDB, LS2080ARDB images, No prebuilt image for FRDM-LS1012a. Attaching the screen shot of the Folders in the mounted images.
Could some one please point me to the FRDM prebuilt image location ?
Thanks
Abhilash
The SDK 2.0 supports the FRDM-LS1012a board if QorIQ Linux SDK v2.0-1703 update is installed. If this update is installed, SDK 2.0 provides building image for the FRDM-LS1012a board.
Use LSDK for loading prebuilt image for the FRDM-LS1012a board:
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------