Differences in Debugging mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences in Debugging mode

821 Views
matanhasan
Contributor I

hi!
I've got two computers with KDS on them, and trying to debug my MCU (MK10FN1M0VLQ12).

in one PC I've got the error : "Could not find core in Coresight setup",
and in the second one I've got the error: "Failed to unsecure Kinetis device".


I've checked the debug configurations in both of the computers, and found that they are the same, so i'm wandering what might be the problem.

thank you!

0 Kudos
2 Replies

456 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Matan Hasan,

It seems your chip is secured.

Which debug probe do you used ? Please unsecure it firstly.

BR

Alice

0 Kudos

456 Views
matanhasan
Contributor I

Yes, i tried that ->
secured & mass erase disabled Kinets MK10FN1M0XXX12 
this is a new thread.

0 Kudos