I cant install S32 Design Studio for ARM v2.0 on Windows 7.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I cant install S32 Design Studio for ARM v2.0 on Windows 7.

2,081 Views
geniusxiong
Contributor I

Hi,

 

I cant install S32 Design Studio for ARM v2.0  on Windows 7.

There is a error entry in the installation log:

Install Uninstaller: S32 Design Studio for ARM v2.0(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

 

I have tired to run the installation as a normal user as well as administrator (Right click -> Run as Administrator). But installation still fails.

 

Is there a solution for this?

Thanks

Sean Lin

0 Kudos
8 Replies

1,436 Views
xiehao5
Contributor I

Hi 天雄 林,

Please check the windows service "Server" status.

Installanywhere relies on the service.

Make sure the "Server" service is enabled and running.

Then retry the installation.

0 Kudos

1,436 Views
medhedibasly
Contributor III

Hello,

i'm having the same issue with "S32DS_Power_Win32_v2017.R1_b171019", is there a solution ?

Regards,

0 Kudos

1,436 Views
geniusxiong
Contributor I

Hi

I tried a lot of method, but couldn't solve the problem, and finally installed win10

0 Kudos

1,436 Views
stanish
NXP Employee
NXP Employee

Hi Sean,

I'd strongly recommend you to install the latest version of S32DS (there is also the update 1  available).

It includes some new features and bug fixes.

S32 Design Studio for ARM 2018.R1 (Windows/Linux) released! 

S32 Design Studio for ARM 2018.R1 - Update 1 available 

Also please try to remove broken installation folder, close all other programs, and re-run the downloaded installer without admin rights.

Please attach the log from this version if the problem persists.

Thanks,

Stan

0 Kudos

1,436 Views
james4
Contributor I

I have the same issue with installing S32DS_ARM_v2.2,the  active  license license couldn‘t popup  and it  rolled back,is there a solution?

0 Kudos

1,436 Views
geniusxiong
Contributor I

Hi Stan,

First thanks for your help.

I tried to install the latest version of S32DS but the problem persists...

And I paste the log, wait for your help.

log:

Installation: Unsuccessful.

19 Successes
0 Warnings
1 NonFatalErrors
1 FatalErrors

Action Notes:

None

Install Log Detail:

Check Disk Space: C:\NXP\S32DS__v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 14,434,590,720

Check Disk Space: C:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 14,434,590,720

Check Disk Space: D:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 10,664,316,928

Install Directory: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL

Install JRE: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL

Install Directory: C:\Users\geniusxiong\AppData\Local\Temp\669755.tmp\
Status: SUCCESSFUL
Additional Notes: NOTE - Directory already existed

Execute Command: NET SESSION
Status: SUCCESSFUL

Execute Command: ping 1.1.1.1 -n 1 -w 10000
Status: SUCCESSFUL

Install Uninstaller: S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
Status: SUCCESSFUL

Install Directory: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\
Status: SUCCESSFUL

Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\iawin32.dll
Status: SUCCESSFUL

Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\win64_32_x64.exe
Status: SUCCESSFUL

Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\remove.exe
Status: SUCCESSFUL

Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\invoker.exe
Status: SUCCESSFUL

Install Uninstaller: S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall Folder: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL

Uninstall Folder: D:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL

Remove Registry Entry: 5 HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\null
Status: SUCCESSFUL

Error occurred while installing the following Action, hence rolling back the installation....!


Action Name: Trigger Rollback Action
Action Description: Trigger Rollback Action


Error Details as below:


This action rolls back the Installation.
====================STDERR ENTRIES==================

__________________________________________________________________________

InstallAnywhere 2014 SP1
Version: 16.5
__________________________________________________________________________

Wed Apr 04 08:57:42 CST 2018

Free Memory: 10547 kB
Total Memory: 15872 kB

No Arguments

Thanks,

Sean Lin

0 Kudos

1,436 Views
stanish
NXP Employee
NXP Employee

Sean,

have you been able to enter your activation code (see below) during the installation?

pastedImage_1.png

0 Kudos

1,436 Views
geniusxiong
Contributor I

Hi Stan,

No, I did not go into this process.

Thanks,

Sean Lin 

0 Kudos