AnsweredAssumed Answered

Running from internal RAM on DSC 56800/E

Question asked by Elvis Memphis on Mar 29, 2018
Latest reply on Apr 1, 2018 by xiangjun.rong

I am working with the 56800/E parts and want to put a small piece of code in RAM. However, in the "DSP56800E and DSP56800EX Core Reference Manual", pg. 8-23, section "8.6 Executing Programs from Data Memory", it seems that the whole application has to go into flash (vectors too) and then configure the part to execute from Internal RAM only.

 

Is it an all or nothing deal when running from internal RAM on the DSC controller?

Outcomes