AnsweredAssumed Answered

CW 8.3 56800/E add second s-record and\or symbol table to debug session

Question asked by Elvis Memphis on Mar 27, 2018
Latest reply on Mar 29, 2018 by ZhangJennie

The DSC 56F800 debugging seems very primitive.

 

In CW 8.3 (and CW 10.7 as well) I do not see how to add a second s-record to flash in the debug session. Further, I do not see a method to load a second symbol table. These features are very useful when debugging bootloader & application scenarios.

 

Also, I do not find any discrete control for how much flash to erase (sector control). The flash programmer that comes with CW 8.3 does provide unit, all, or page. That is helpful but still pretty course.

 

What are the steps to add a second s-record or a symbol table to an existing debug session?

Outcomes