AnsweredAssumed Answered

MPC5748,Flex CAN0,1,2 works on Z4_0Core,CAN 3,4,5 on Z4_1,CAN6,7 on Z2

Question asked by jianping lan on Mar 24, 2018

sorry,my english is poor.

In my project,I need to deal with eight can signals with a lot of data.So, I want to get the Z40 core to handle the can0-2 ,Z41 handle the 3-5,the others on z2.When multiple cores work at the same time, the phenomenon of Z4O program running away will occur. The 8-way can works without a problem with one core.Are there any relevant examples for reference?

Outcomes