PTN3460 Programming over AUX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3460 Programming over AUX?

1,738 Views
danielgloeckner
Contributor I

Is there any way to change the settings stored in the internal flash (f.ex. the emulated EDIDs) over AUX while the chip is in I2C slave mode?

Tags (1)
0 Kudos
8 Replies

616 Views
MaxxCO
Contributor I

Hello, 
Any updates here? I am also wondering if the EDID can be programmed thru I2C-over-AUX channel and if YES, what else is needed ( additional NXP software, or any special additional hardware ) ? 
Thanks

0 Kudos

617 Views
MaxxCO
Contributor I

Hi, 
Are there any updates on the above posted question?

0 Kudos

1,191 Views
guoweisun
NXP TechSupport
NXP TechSupport
Hi
PTN3460 is built in a configuration table in internal SRAM, which allows user to program seven EDID and 128 configuration registers through M/S I2C-bus.

Please find the link for Application note AN11128 “PTN3460 Programming detail.
0 Kudos

1,191 Views
danielgloeckner
Contributor I

I am well aware that the configuration can be changed over M/S I2C.

But I want to know if it is possible to do this over AUX.

0 Kudos

1,191 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

I am afraid that you can't ,you can only over Flash to AUX tool to update the PTN3460 firmware.

0 Kudos

1,191 Views
danielgloeckner
Contributor I

It was pointed out to me that section 8.3.9 of the PTN3460 data sheet says that it should be possible to program the EDID over AUX:

Given that EDID is specific to panels, PTN3460 enables system integrator to program EDID information into embedded memory through DP AUX and I2C-bus interfaces.

Is that an error in the data sheet?

0 Kudos

1,191 Views
guoweisun
NXP TechSupport
NXP TechSupport

It is IIC Over AUX operation not IIC and AUX.

0 Kudos

1,191 Views
sborden
Contributor I

Can a standard EDID programmer be used?

0 Kudos