AnsweredAssumed Answered

Build binarys for mfgtool and i.MX RT1050 EVK

Question asked by René Lüllau on Mar 21, 2018
Latest reply on Dec 22, 2018 by Jay Heng

Hello.

 

I have an I.MX RT1050 Evaluation Kit that I want to flash with the mfgtool and a binary from MCUxpresso. The flash memory I want to use is the QSPI Flash of the Kit and not the HyperFlash. By now I was only able to generate a flash-able boot image of the prebuild hello world project of the SDK but i couldn't build a binary that boots by myself.

 

I build a binary with checksum and the flash start address at 0x60002000. After that i used that binary to build a boot image with elftosb and followed the steps described in this document at chapter 4.2.

 

I used the "program_flexspinor_image_qspinor.bd" file that is already in the bd_file directory, i made a custom bd file like it is explained in the manual at chapter 4.2 and i used the bd file that is attached in this post. Everything with the flash start address at 0x60002000 and at 0x60000000 with the bin files and the afx files.

I also edited the "fsl_flexspi_nor_flash.c" file like it is described here.

 

I never got an error at flashing the RT1050 but my image didn't booted neither.

 

I think there are some Build Settings I missed to set properly or the bd files I used aren't correct.

Outcomes