IMX6 BAR0 EXTEND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 BAR0 EXTEND

563 Views
bluesky507
Contributor I

I checked pci driver sources provided for IMX.6 CPU. It seems that ddr memory window reserved for root complex is limited to 16M. I need at least 256M for BAR0 in my application. Is it possible to patch the driver to support such memory size?
Thanks

0 Kudos
2 Replies

475 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Only 16 MB address range is available for PCIe in i.MX6 system memory map.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

475 Views
bluesky507
Contributor I

I need cor board can support 256mbyte pcie memory space.

can you help me to find?

0 Kudos