AnsweredAssumed Answered

SDHC Class 10 Boot -Processor Part Number?

Question asked by balaji padmanaban on Mar 12, 2018
Latest reply on Mar 12, 2018 by igorpadykov

Can somebody Suggest a Processor which can have a SDHC card has a boot interface?

UART-3

SPI-2

ADC-2.

JTAG

ADC-2

Secondary Boot

SRAM min-512KB

SDHC-Transfer speed 10MB/s should support class 10

 

----------------

DDR2- if available not manadatory

 

 

I see no micro controller doing SDHC boot from my trade study.

But a micro controller is can do all except SDHC boot with boot options to the next boot device no bootstrap is available on it?.

 

Any help or suggestions of part numbers?

Outcomes