AnsweredAssumed Answered

Can't find PMIC:PFUZE100

Question asked by Yoshihisa Saito on Mar 9, 2018
Latest reply on Mar 14, 2018 by Yoshihisa Saito

Hi,

 

processor:   MX6Q;

Board     :   SabreAI rev.A

BSP:      :   L4.9.11_1.0.0 (Build by myself) 

                     L4.9.11_1.0.0 (Download demo file)

                    L3.14.52 (Download demo file)

 

I started it with the above configuration.
However, the following error occurred.
How can I solve it?
Is the board broken?

 

=======

Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Dec 05 2015 - 02:02:30)

CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 25 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 2 GiB
Can't find PMIC:PFUZE100
initcall sequence 8ff8e124 failed at call 178036b0 (err=-19)
### ERROR ### Please RESET the board ###

=======

 

Best regards,
Yoshihisa Saito

Outcomes