Hi, I like to test LPC4370 ADCHS capability , first I need to apply an analog input signal to LPC-link2 board, then I will practice with LPC4370 configuration and coding to test the ADCHS functionality. I look the LPC-link 2 schematics and other document, but I am not sure where is the input pin for ADCHS。
From Schematics , I see ADC input on J4 , asshown below.
but I do not see the corresponding I/O on LPC4370 I/O, also on Schematics.
Can someone tell me,
1. Whether I can apply a signal in LPC link2 ,and gets to the LPC4370 ADCHS input ?
2. If I can, where and how ?
Best Regards,