Hi,
My customer board u-boot was corrupted due to incorrect u-boot flashing from update procedure. Now board is not booting. So i am using MFGTool to re-flash my default u-boot to board. But u-boot loading will stop at the midway, We are not able to identify the reason that causing this abort at midway.
Any thoughts regarding this?
Please find attached screenshots of the MFGTool while flashing the u-boot.
Hi sadasivappa
for custom board it is necessary to run ddr test
i.MX6/7 DDR Stress Test Tool V3.00
and rebuild mfg tool firmware (files in /firmware folder)
with new calibration coefficients set in uboot/../freescale/board/board_name/*.cfg
file. Please use sect.6.2 Manufacturing Tool, MFGTool attached Yocto
Guide. Use corresponding mfg tools version the same as bsp version from link
i.MX Software|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------