AnsweredAssumed Answered

Problems to use MfgTool with IMXRT1050-EVBK

Question asked by Angelo Bertuletti on Mar 7, 2018
Latest reply on Dec 22, 2018 by Jay Heng

I have problems with the software MfgTool when I try to flash the IMXRT1050-EVBK.

I want store the example "emWin".

 

If I open it as it is, after downloading it from the NXP site, the software doesn't detect the dev-board (see image SW_Original.jpg)
If I open it, after change the VID and the PID of the file ucl2.xml (the same of the driver mbed), the dev-board is detected, but the programming procedure doesn't work (see image SW_Modified.jpg)
The error is:
"Boot" body = "BootStrap" error, file = "C:\Flashloader_RT1050_1.0\Tools\mfgtools-rel_emwin\Profiles\MXRT105X\OS Firmware\ivt_flashloader.bin"
I have attached also the LOG generated by MfgTool.

 

Thanks in advance,
Angelo

Attachments

Outcomes