Hi,
I am trying to run ddr callibration in imx6dl and it is getting failed with the following error,
# DDR_Stress_Tester.exe -t mx6x -df imx6dl-custom.inc
MX6DL opened.
HAB_TYPE: DEVELOP
rom_write: reading HAB ack failed 0x00000000
ROM Write failed, addr: 0x021b001c
Write dcd failed.
#
We are using DDR3-1333 part no: IS46TR16256A-15HBLA2-TR.
Please find the attached ddr3 script aid configuration.
Kindly help us to find out what is wrong with the configuration.
Regards,
Abdul
Hi Abdul
please try latest gui version of tool, use description in presentation and look at FAQ on below link
Q. I see an error message that states "ERROR: DCD addr is out of valid range.",
i.MX6/7 DDR Stress Test Tool V3.00
DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------