eMMC update on CL-SOM-IMX8?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC update on CL-SOM-IMX8?

Jump to solution
1,073 Views
byunggukchoi
Contributor II

I bought a CL-SOM-IMX8 reference board.

And I'm trying to update kernel on u-boot but I don't know the exact block number for kernel image and dtb to locate in MMC.

In the following command, 0x5000 for kernel image and 0xE000 for dtb are arbitrary block numbers.

I want to know the exact block number instead of 0x5000 and 0xE000 for kernel and dtb.

u-boot=> tftp 0x40480000 Image

u-boot=> tftp 0x43000000 cl-som-imx8.dtb

u-boot=> mmc write 0x40480000 0x5000 0x9000

u-boot=> mmc write 0x43000000 0xE000 0x800

Thanks in advance.

Labels (4)
0 Kudos
1 Solution
625 Views
igorpadykov
NXP Employee
NXP Employee

Hi ByungGuk

for programming one can use mfg tools (for details please check included ucl2.xml)

https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_Beta_MFGTOOL&appType=license&location=nul... 

and Linux L4.9.51 8MQuad Beta Documentation

https://www.nxp.com/webapp/Download?colCode=L4.9.51_8MQ_BETA_LINUX_DOCS 

Best regards
igor
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
626 Views
igorpadykov
NXP Employee
NXP Employee

Hi ByungGuk

for programming one can use mfg tools (for details please check included ucl2.xml)

https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_Beta_MFGTOOL&appType=license&location=nul... 

and Linux L4.9.51 8MQuad Beta Documentation

https://www.nxp.com/webapp/Download?colCode=L4.9.51_8MQ_BETA_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos