AnsweredAssumed Answered

USB Automounting fails

Question asked by David XY Zhou on Mar 5, 2018
Latest reply on Mar 5, 2018 by Victor Linnik

Hi,

 

I have imx6ul development board with Linux 4.15.

 

I found there is a problem with USB automounting (USB 2.0 memory stick). The same type USB sticks, some of them work well with automounting and others don't. With the sticks failed automounting, they can be mounted manually. Here are  observations:

1. Good ones don't show up the messages:

    [sda] No Caching mode page found                
    sd 1:0:0:0: [sda] Assuming drive cache: write through
2. Bad ones always display the above messages when they are plugged in.

3. if udevadm monitor is running, all of them are auto-mounted successfully.

 

The link :

[SOLVED] USB drives no longer being auto mounted [Archive] - Ubuntu Forums 

It seems provide a solution for that similar problem, but I found no modules file under /etc folder for yocto/linux.

 

Can anyone propose a solution?

 

Thank you

David Zhou

Outcomes