Hi everyone,
I'm developing an application using a custom board based on MK66, MCUXpresso 10.1.1 and SDK 2.3.
On the board there is external battery backed up RAM, used for a ramdisk, and a 8 MB dataflash device (AT45DB321E), where I need to implement 2 different disk.
I've read the FatFs docs and it seems that I can handle only 1 disk of the same type (ramdisk, SD disk, MMC disk).
Did I misunderstand something?
How can I handle my devices?
Many thanks
Biafra
Hi Biafra:
In theory it is possible to write into several different physical discs, but I have never tried it in practice.
Regards
Daniel