TWR-LS1021A Flash Programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-LS1021A Flash Programming

824 Views
christopherbisc
Contributor II

I am working with an LS1021A CPU on a customized board based on the TWR-LS1021A reference board.

For programming the Flash I am using Codewarrior USB Tap and CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA IDE.

Is there any possibility to program the Flash without the CodeWarrior Development Studio and the corresponding license for the production flow. Like a Standalone programmer, or a free version of Codewarrior?

0 Kudos
1 Reply

602 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Christopher Bischof,

There is a 30 days free evaluation license for the customer to use CodeWarrior.

For LS1021A custom board bringing up and flash programming, the customer needs to purchase the Developer Level Suite.

Except using CodeWarrior, you also could consider to set up SD/MMC u-boot, then program flash under SD u-boot.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos