MY-IMX6-EK140(i.MX6ul)
Development board are made up of devices below:
Development board accessories
MY-IMX6-EK140 is standard,no accessories.The complimentary part is below:
Development board optional accessories
EK140 Front View
EK140 Rear View
MY-IMX6-EK140 interface
No. | Interface | Function | Interface form | Silk screen |
1 | USB OTG | MFG Tool burning input port and USB OTG | Micro USB | J4 |
2 | ENET | 10/100-Mbps ethernet | RJ-45 | P1 |
3 | 5V_IN | power in | Micro USB | J3 |
4 | 5V_IN | power in | single row pin( 2pins) | J2 |
5 | DEBUG UART | debug serial port | singla row pin(4 pins) | J1 |
6 | BOOT Device | boot device option | dial switch (4bit) | SW1 |
7 | TF | TF card | TF card boot(flip type) | U2 |
8 | LCD DISPLAY | LCD display interface | FPC socket(flip type,40pins) | U1 |
9 | BOOT MODE | boot mode option | dial swtich(2bit) | SW2 |
10 | RESET | reset button | key(2 pins) | SW3 |
11 | FXLS8471Q | acceleration sensor | none | U8 |
12 | FXAS21002CQ | 3D digital gyroscope | none | U10 |
13 | MAG3110 | 3D magnetic sensor | none | U9 |
14 | TS | resistance touch screen interface | PFC socket(drawer-type,4 Pin | J5 |
15 | J6 | function socket | dual row socket | J3 |
16 | J7 | function socket | dual row socket | SW1 |
17 | USER LIGHT | user LED light | LED light(4 units) | D* |
18 | POWER LIGHT | power indication light | LED light(2 units) | D* |
Application Area:
Robot and Industrial automation
Linux systems with hard real-time functions are integrated with industrial interfaces such as CAN and RS485. MY-I.MX6 module is an ideal solution for robot and industrial automation applications. It can be implemented more quickly and flexibly on Linux. Or using a variety of available GPIOs, connect to your visual system via a camera interface, or safely back up the data in the process through the Ethernet cloud. Whatever your application is, We are pleased to provide product consulting services when you select the appropriate MY-I.MX6 computer module.
Voyage
Harsh anti vibration and can operate in industrial temperature range, has been the ship equipment used to select computer module prerequisites for our products by customers. The module is integrated into the sonar system, fleet management, communication unit and marine diesel engine controller. MY-I.MX6 core module also can meet the most stringent requirements of marine certification agency.
Laboratory equipment
From mass spectrometers to electronic scales. MY-I.MX6 core modules can be widely used in scientific laboratory instrumentation products of market leaders in their respective fields. Depending on the functionality, processing power, and interfaces you need for the device you are designing. Or the amount of memory may be an important feature of the modular product you choose. Do you need to output to a particular type of display or do the product receive data from different types of sensors? For each of these modules, you need to select a different feature. You may need a touch screen interface, a camera interface for USB hosts and clients, and multiple SD card interfaces. Internal solid state storage, etc. Please contact us, we will tell you which modules best meet your requirements.
Retail & Ticketing
Electronic scale, bar code reader, inventory management system and cash register, core modules can also be used in the array of retail equipment
A large number of tickets are allocated and used in parking lots, toll roads and other places. Not only for the tickets, but also for collecting the appropriate fees at the same time of recycling, the commonly used water heaters and coffee machines in restaurants, catering facilities can help guests get their required
Medical & Health care
From hospital monitoring to home care, embedded computers are widely used in the field of medical devices. Do you want to get complex results from graphics that are easy to understand on the screen? Or, you need to compute the data from a variety of sensors. Either way, the MY-I.MX6 core module is designed and manufactured according to the principle of maximum reliability. Many of our industry-leading customers have successfully obtained 3C and CE products certification
Environmental monitoring
Although the MY-I.MX6 core module is powerful in computing, it has very low energy consumption and no fan applications. They are perfect solution for handheld devices, low maintenance remote systems or smart sensors. Various sensor input channels, coupled with the advantages of easy connectivity to common networks and low power consumption. Make MYZR series module as the best choice for outdoor environmental monitoring applications, such as tsunami warning system. This module is for many interfaces, such as I2CU SPI. RS232 and others provide convenient connections.
If you would like to know more about our products, please visit www.myzr.com.cn or email to enquiry@myzr.com.cn.