Hi I'm new to i.MX and currently have problems using the fsl-community-bsp source code. I'm using the i.MX 7Dual Sabre Board for Smart Device.i.MX 7Dual SABRE Board|NXP
I want to build the image (uboot, kernel, etc) for my board, at least to have my board functioning properly.
What is the suitable bitbake target for imx7dsabre board?
What I have done is:
#install repo
mkdir ~/bin
curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
chmod a+x ~/bin/repo
#Download the source code
PATH=${PATH}:~/bin
mkdir fsl-community-bsp
cd fsl-community-bsp
repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b rocko
repo sync
#config board
MACHINE=imx7dsabresd DISTRO=fslc-framebuffer source setup-environment build/
#build target
bitbake core-image-minimal
But fetch failure always happens during the building process and thus error is encountered.
Btw, I have tried using the linux-imx.git and u-boot-imx.git before. The building process is fine and the output image works well. But I was stuck in how to add a custom application layer to the src code.
Please advise and thanks :smileygrin: