AnsweredAssumed Answered

Glueless interface of SDRAM with MPC8270

Question asked by TOL TOL on Feb 28, 2018
Latest reply on Mar 11, 2018 by alexander.yakovlev

Hi i am using 12 SDRAMs with my MPC8270 and it says that it uses glues-less interface of SDRAM and other peripherals. 

Because of 12 SDRAM i am not able to do use my bus at 100Mhz because of signal integrity issues. As load is too high and 60x bus is not able to drive the SDRAM.

So can i use buffers in between SDRAM and PowerPC MPC8270?

I am confused because it says glue less interface, so is glue less interface must or optional?

Outcomes