QN9080 USB Dongle Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080 USB Dongle Firmware

Jump to solution
1,259 Views
bmhuerta
Contributor I

Where can I find the latest firmware version for the QN9080 dongle? Apparently it should appear in the QTool installation directory, but I can not find it. I'm using the QTool Rev. 1.0.0, released on 2018-02-01.

Labels (1)
Tags (3)
0 Kudos
1 Solution
753 Views
anthony_huereca
NXP Employee
NXP Employee

Hi,

  The new firmware is now available as part of the updated QTool installation package. It can be found in the "bin files" directory. https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup 

  To update the dongle firmware, short TP5 to ground (you can use the USB shield) and press the reset button. You should see a "CRP DISABLD" drive enumerate. Delete the firmware.bin file in that drive, and then drag-and-drop the new firmware.bin file into that drive. 

-Anthony 

View solution in original post

0 Kudos
2 Replies
754 Views
anthony_huereca
NXP Employee
NXP Employee

Hi,

  The new firmware is now available as part of the updated QTool installation package. It can be found in the "bin files" directory. https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup 

  To update the dongle firmware, short TP5 to ground (you can use the USB shield) and press the reset button. You should see a "CRP DISABLD" drive enumerate. Delete the firmware.bin file in that drive, and then drag-and-drop the new firmware.bin file into that drive. 

-Anthony 

0 Kudos
753 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Borja,

  The QTool software is being updated very soon to include the firmware. I'll post back when the new version is available. 

-Anthony 

0 Kudos