Does IMX6 SOLO is capable of supporting 2GB RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does IMX6 SOLO is capable of supporting 2GB RAM

873 Views
manojsampathkum
Contributor II

Hi

In our design, we are planning to use imx6 solo with 2gb ram but regarding the capacity of RAM  supported I couldn't able to find out in TRM. Can SOLO processor support 2GB ram? If it supports what are the procedure I need to follow to make it work?

Regards 

Manoj

Labels (2)
2 Replies

673 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 

  You may use AN4397 (Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite)

regarding differences of devices of i.MX6 series.

 

http://cache.nxp.com/files/32bit/doc/app_note/AN4397.pdf

 

  In particular, take a look at Table 2 (Summary of feature differences). Memory is supported practically

up to 4GBytes.

   Please refer to "i.MX_BSP_Porting_Guide.pdf" of Linux documentation how to configure memory

in U-boot.

 

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

673 Views
manojsampathkum
Contributor II

thanks for the support.

0 Kudos