AnsweredAssumed Answered

Can We Use 933MHz or 1GHz Memory instead of 800MHz Memory For iMAX6Q HW Design ?

Question asked by Peter Amond on Feb 27, 2018
Latest reply on Mar 23, 2018 by Thorsten Wronski

Hi All,

 

I'm using iMAX6Q processor based hardware design which is most similar to nitrogen6_max development board.

 

I used 800MHz 4Gb 256M x 16 Alliance memory module for my original design. Manufacturer part number - AS4C256M16D3A-12BCN (800MHz)

 

Due to the end of life reason I'm going to shift for following Micron memory modules. 

 

MT41J256M16LY-091G:N  -  SDRAM - DDR3 Memory IC 4Gb (256M x 16) Parallel 1GHz 96-FBGA  (933MHz)

MT41K256M16TW-107 AAT:P  -  SDRAM - DDR3L Memory IC 4Gb (256M x 16) Parallel 933MHz 20ns 96-FBGA (8x14)   (1GHz)

 

Is there any conflict to use above memory modules with my hardware design (With iMAX6Q processor)?

 

Regards,

Peter.

Outcomes