Hi All,
I'm using i.MX6 sabresd DL for my cpu and linux kernel driver for version 4.1.15.
I'm trying to display the monitor via USB.
Which driver I should open and build in?
And what else I have to do ?
Thanks in Advance!
Hi victor
seems one needs to implement support for usb monitor driver described on
http://www.usb.org/developers/docs/devclass_docs/usbmon10.pdf
Chapter 39 CHIPIDEA USB Driver attached Linux Manual describes
current lnux usb driver capabilities.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is this just can support X86 structure CPU ?
Or I can using on the ARM structure?