chayma barka

NXP Model-Based Design Tools

Discussion created by chayma barka on Feb 22, 2018
Latest reply on Mar 2, 2018 by chayma barka

Hello, 
I'm working on TWR-KV10Z32 eval board, and i'm using Motor Control Toolbox on Simulink to generate code. 
I would like to generate an interrupt when there's a timer overflow, but the bloc that enables that interrupt, attached in the figure below, can only enable the interrupt for module 1 and 2, while i'm using FTM0 (Module 0). 

In the help, it's mentionned that i can configure module 0

 

What  can i do to generate the FTM0 overflow interrupt? 

 

Thank you for your support.

Outcomes