I compile android with the flag build_device_target=sd, the first boot all goes well but if i reboot or shutdown i have the following errors in partitions, I attach the log, How can I solve it?
U-Boot SPL 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)
SPL: u-boot second stage will be loaded from MMC0
U-Boot 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 38 C
Reset cause: WDOG
Board: UDOO Quad
Watchdog enabled
DRAM: 1 GiB
MMC: FSL_SDHC: 0
*** Warning - bad CRC, using default environment
auto-detected panel HDMI
Display: HDMI (1280x720)
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:0
Net: using phy at 6
FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 3 2 1 0
112 bytes read in 148 ms (0 Bytes/s)
Running bootscript from mmc ...
Device Tree: dts/imx6q-udoo-hdmi.dtb
42833 bytes read in 86 ms (486.3 KiB/s)
boota mmc0
kernel @ 14008000 (5719992)
ramdisk @ 15000000 (917604)
fdt @ 14f00000 (42833)
## Booting Android Image at 0x12000000 ...
Kernel load addr 0x14008000 size 5586 KiB
Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
Loading Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f0d750
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 3.14.52-09424-g6fe6e7b-dirty (root@eyenai-VirtualBox) (gcc version 5.3.1 20160401 (optimized) (UBERTC-5.3.x) ) #1 SMP PREEMPT Wed Feb 7 21:19:47 CET 2018
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: UDOO Quad Board
[ 0.000000] cma: CMA: reserved 256 MiB at 2e000000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] PERCPU: Embedded 8 pages/cpu @ee741000 s8640 r8192 d15936 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260384
[ 0.000000] Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend androidboot.serialno=0c09a1d4e3173fe7
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 763932K/1047552K available (7132K kernel code, 439K rwdata, 2408K rodata, 288K init, 497K bss, 283620K reserved, 277504K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xef800000 - 0xff000000 ( 248 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef000000 ( 752 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0959514 (9542 kB)
[ 0.000000] .init : 0xc095a000 - 0xc09a21c0 ( 289 kB)
[ 0.000000] .data : 0xc09a4000 - 0xc0a11d80 ( 440 kB)
[ 0.000000] .bss : 0xc0a11d8c - 0xc0a8e400 ( 498 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] L310 cache controller enabled
[ 0.000000] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB
[ 0.000000] Switching to timer-based delay loop
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
[ 0.000816] Console: colour dummy device 80x30
[ 0.000840] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.000853] pid_max: default: 32768 minimum: 301
[ 0.000956] Security Framework initialized
[ 0.001010] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001022] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001663] Initializing cgroup subsys debug
[ 0.001676] Initializing cgroup subsys freezer
[ 0.001701] CPU: Testing write buffer coherency: ok
[ 0.001952] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002006] Setting up static identity map for 0x106cebc0 - 0x106cec18
[ 0.060999] CPU1: Booted secondary processor
[ 0.061020] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080985] CPU2: Booted secondary processor
[ 0.081005] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.100984] CPU3: Booted secondary processor
[ 0.101004] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.101103] Brought up 4 CPUs
[ 0.101132] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[ 0.101141] CPU: All CPU(s) started in SVC mode.
[ 0.101568] devtmpfs: initialized
[ 0.105161] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.105482] pinctrl core: initialized pinctrl subsystem
[ 0.105789] regulator-dummy: no parameters
[ 0.120425] NET: Registered protocol family 16
[ 0.128269] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.128813] cpuidle: using governor ladder
[ 0.128823] cpuidle: using governor menu
[ 0.129213] CPU identified as i.MX6Q, silicon rev 1.2
[ 0.129339] Use WDOG1 as reset source
[ 0.136255] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
[ 0.136525] vdd1p1: 800 <--> 1375 mV at 1100 mV
[ 0.136844] vdd3p0: 2625 <--> 3400 mV at 3000 mV
[ 0.137153] vdd2p5: 2000 <--> 2750 mV at 2400 mV
[ 0.137446] vddarm: 725 <--> 1450 mV at 1150 mV
[ 0.140361] vddpu: 725 <--> 1450 mV
[ 0.140687] vddsoc: 725 <--> 1450 mV at 1175 mV
[ 0.142467] syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
[ 0.144580] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
[ 0.147985] apx_wdog trigger loaded
[ 0.148004] apx_wdog: enabled wdog - 0 s between refresh
[ 0.148884] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.148894] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.149526] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.170971] bio: create slab <bio-0> at 0
[ 0.172857] mxs-dma 110000.dma-apbh: initialized
[ 0.173465] usb_h1_vbus: 5000 mV
[ 0.173658] usb_otg_vbus: 5000 mV
[ 0.173845] 2P5V: 2500 mV
[ 0.174184] i2c-core: driver [max17135] using legacy suspend method
[ 0.174193] i2c-core: driver [max17135] using legacy resume method
[ 0.174709] SCSI subsystem initialized
[ 0.175135] usbcore: registered new interface driver usbfs
[ 0.175197] usbcore: registered new interface driver hub
[ 0.175290] usbcore: registered new device driver usb
[ 0.175411] usbphy_nop1.11 supply vcc not found, using dummy regulator
[ 0.175500] usbphy_nop2.12 supply vcc not found, using dummy regulator
[ 0.176640] i2c i2c-1: IMX I2C adapter registered
[ 0.177441] i2c i2c-2: IMX I2C adapter registered
[ 0.177551] Linux video capture interface: v2.00
[ 0.177593] pps_core: LinuxPPS API ver. 1 registered
[ 0.177602] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.177625] PTP clock support registered
[ 0.190411] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.210392] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.211479] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
[ 0.211493] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
[ 0.211555] MIPI CSI2 driver module loaded
[ 0.211633] Advanced Linux Sound Architecture Driver Initialized.
[ 0.212692] Loading modules backported from Linux version v4.1.7-0-g0c5c1f1
[ 0.212701] Backport integrated by backports.git v4.1.1-1-0-g8286954
[ 0.212710] Bluetooth: Core ver 2.20
[ 0.212763] NET: Registered protocol family 31
[ 0.212773] Bluetooth: HCI device and connection manager initialized
[ 0.212788] Bluetooth: HCI socket layer initialized
[ 0.212802] Bluetooth: L2CAP socket layer initialized
[ 0.212835] Bluetooth: SCO socket layer initialized
[ 0.213269] Switched to clocksource mxc_timer1
[ 0.222379] NET: Registered protocol family 2
[ 0.223192] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.223298] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.223425] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.223500] TCP: reno registered
[ 0.223514] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.223554] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.223792] NET: Registered protocol family 1
[ 0.224013] Trying to unpack rootfs image as initramfs...
[ 0.277366] Freeing initrd memory: 896K (c5000000 - c50e0000)
[ 0.277980] hw perfevents: enabled with ARMv7_Cortex_A9 PMU driver, 7 counters available
[ 0.278712] imx_busfreq busfreq.15: DDR medium rate not supported.
[ 0.279145] Bus freq driver module loaded
[ 0.280340] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.281969] bounce pool size: 64 pages
[ 0.287125] VFS: Disk quotas dquot_6.5.2
[ 0.287373] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.288706] NTFS driver 2.1.30 [Flags: R/W].
[ 0.289150] fuse init (API version 7.22)
[ 0.289543] msgmni has been set to 1463
[ 0.292252] NET: Registered protocol family 38
[ 0.292291] io scheduler noop registered
[ 0.292301] io scheduler deadline registered
[ 0.292335] io scheduler cfq registered (default)
[ 0.292763] imx-weim 21b8000.weim: Driver registered.
[ 0.294263] MIPI DSI driver module loaded
[ 0.295305] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[ 0.295335] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[ 0.295423] mxc_sdc_fb fb.20: registered mxc display driver hdmi
[ 0.333349] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 0.402863] Console: switching to colour frame buffer device 240x67
[ 0.442896] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[ 0.443457] imx-sdma 20ec000.sdma: no event needs to be remapped
[ 0.443904] imx-sdma 20ec000.sdma: loaded firmware 3.3
[ 0.446417] imx-sdma 20ec000.sdma: initialized
[ 0.446827] Serial: IMX driver
[ 0.447191] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
[ 1.294951] console [ttymxc1] enabled
[ 1.295359] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
[ 1.295645] serial: Freescale lpuart driver
[ 1.296645] [drm] Initialized drm 1.1.0 20060810
[ 1.297014] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[ 1.303896] brd: module loaded
[ 1.307567] loop: module loaded
[ 1.308036] zram: Created 1 device(s) ...
[ 1.308370] [bossac] Registering IRQ 323 for BOSSAC Arduino erase/reset operation
[ 1.308596] [bossac] Created device file /dev/udoo_ard
[ 1.309441] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[ 1.309449] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[ 1.309455] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[ 1.309461] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[ 1.313090] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[ 1.313121] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 1.313132] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 1.314905] scsi0 : ahci_platform
[ 1.315164] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
[ 1.317254] tun: Universal TUN/TAP device driver, 1.6
[ 1.317257] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 1.317420] CAN device driver interface
[ 1.318343] 2188000.ethernet supply phy not found, using dummy regulator
[ 1.433650] pps pps0: new PPS source ptp0
[ 1.479292] libphy: fec_enet_mii_bus: probed
[ 1.479752] fec 2188000.ethernet eth0: registered PHC device 0
[ 1.479942] PPP generic driver version 2.4.2
[ 1.480132] PPP BSD Compression module registered
[ 1.480135] PPP Deflate Compression module registered
[ 1.480158] PPP MPPE Compression module registered
[ 1.480163] NET: Registered protocol family 24
[ 1.480237] usbcore: registered new interface driver asix
[ 1.480295] usbcore: registered new interface driver ax88179_178a
[ 1.480335] usbcore: registered new interface driver cdc_ether
[ 1.480374] usbcore: registered new interface driver cdc_eem
[ 1.480412] usbcore: registered new interface driver net1080
[ 1.480450] usbcore: registered new interface driver cdc_subset
[ 1.480487] usbcore: registered new interface driver zaurus
[ 1.480563] usbcore: registered new interface driver cdc_ncm
[ 1.480567] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.480571] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 1.480708] usbcore: registered new interface driver cdc_acm
[ 1.480711] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.480767] usbcore: registered new interface driver usb-storage
[ 1.480871] usbcore: registered new interface driver usbserial
[ 1.480912] usbcore: registered new interface driver usbserial_generic
[ 1.480945] usbserial: USB Serial support registered for generic
[ 1.480980] usbcore: registered new interface driver ftdi_sio
[ 1.481011] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.481051] usbcore: registered new interface driver option
[ 1.481083] usbserial: USB Serial support registered for GSM modem (1-port)
[ 1.481126] usbcore: registered new interface driver usb_ehset_test
[ 1.481850] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 1.489807] ci_hdrc ci_hdrc.1: doesn't support gadget
[ 1.489825] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 1.489849] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[ 1.503321] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 1.503516] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.503524] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.503530] usb usb1: Product: EHCI Host Controller
[ 1.503535] usb usb1: Manufacturer: Linux 3.14.52-09424-g6fe6e7b-dirty ehci_hcd
[ 1.503541] usb usb1: SerialNumber: ci_hdrc.1
[ 1.504123] hub 1-0:1.0: USB hub found
[ 1.504155] hub 1-0:1.0: 1 port detected
[ 1.505078] mousedev: PS/2 mouse device common for all mice
[ 1.505598] usbcore: registered new interface driver usbtouchscreen
[ 1.506043] input: st1232-touchscreen as /devices/soc0/soc.0/2100000.aips-bus/21a8000.i2c/i2c-2/2-0055/input/input0
[ 1.506897] snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
[ 1.507176] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
[ 1.507265] i2c /dev entries driver
[ 1.508383] 2-003c supply DOVDD not found, using dummy regulator
[ 1.508430] 2-003c supply DVDD not found, using dummy regulator
[ 1.508467] 2-003c supply AVDD not found, using dummy regulator
[ 1.663455] ata1: SATA link down (SStatus 0 SControl 300)
[ 1.663495] ahci-imx 2200000.sata: no device found, disabling link.
[ 1.663501] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[ 1.698273] ov5640_read_reg:write reg error:reg=300a
[ 1.698275] camera ov5640_mipi is not found
[ 1.699042] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video16
[ 1.699176] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video17
[ 1.699447] usbcore: registered new interface driver uvcvideo
[ 1.699449] USB Video Class driver (1.1.1)
[ 1.699688] [UDOO power-off] Probed LVDS power.
[ 1.699766] [UDOO power-off] Probed LVDS backlight.
[ 1.699833] [UDOO power-off] Probed UDOO Quad/Dual.
[ 1.700242] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
[ 1.700545] device-mapper: uevent: version 1.0.3
[ 1.700867] device-mapper: ioctl: 4.27.0-ioctl (2013-10-30) initialised: dm-devel@redhat.com
[ 1.701226] sdhci: Secure Digital Host Controller Interface driver
[ 1.701229] sdhci: Copyright(c) Pierre Ossman
[ 1.701231] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.706455] mmc0: no vqmmc regulator found
[ 1.706463] mmc0: no vmmc regulator found
[ 1.743312] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[ 1.743945] Warning: No contiguous memory is reserverd for gpu.!
[ 1.743945]
[ 1.743951] Warning: Will use default value(134217728) for the reserved memory!
[ 1.743951]
[ 1.743957] Galcore version 5.0.11.41671
[ 1.823486] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 1.926840] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.945914] mmc0: new high speed SDHC card at address 0007
[ 1.946552] mmcblk0: mmc0:0007 SD32G 29.0 GiB
[ 1.990777] mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
[ 2.001288] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[ 2.001298] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.007164] hub 1-1:1.0: USB hub found
[ 2.011100] hub 1-1:1.0: 4 ports detected
[ 2.258970] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 2.259502] mxc_vpu 2040000.vpu: VPU initialized
[ 2.333535] usb 1-1.1: new low-speed USB device number 3 using ci_hdrc
[ 2.468402] usb 1-1.1: New USB device found, idVendor=0e8f, idProduct=00fb
[ 2.475309] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 2.482648] usb 1-1.1: Product: USB Mouse
[ 2.486679] usb 1-1.1: Manufacturer: YSTEK
[ 2.507187] caam 2100000.caam: Instantiated RNG4 SH0
[ 2.583528] usb 1-1.3: new high-speed USB device number 4 using ci_hdrc
[ 2.731280] usb 1-1.3: New USB device found, idVendor=148f, idProduct=5370
[ 2.738210] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 2.745555] usb 1-1.3: Product: 802.11 n WLAN
[ 2.749622] caam 2100000.caam: Instantiated RNG4 SH1
[ 2.749631] caam 2100000.caam: device ID = 0x0a160100 (Era 4)
[ 2.749638] caam 2100000.caam: job rings = 2, qi = 0
[ 2.765637] usb 1-1.3: Manufacturer: Ralink
[ 2.769831] usb 1-1.3: SerialNumber: 1.0
[ 2.826183] caam algorithms registered in /proc/crypto
[ 2.834987] caam_jr 2101000.jr0: registering rng-caam
[ 2.840872] snvs-secvio 20cc000.caam-snvs: can't get snvs clock
[ 2.846874] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
[ 2.855172] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.866846] input: YSTEK USB Mouse as /devices/soc0/soc.0/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.1/1-1.1:1.0/0003:0E8F:00FB.0001/input/input1
[ 2.881158] hid-generic 0003:0E8F:00FB.0001: input,hidraw0: USB HID v1.10 Mouse [YSTEK USB Mouse] on usb-ci_hdrc.1-1.1/input0
[ 2.892585] usbcore: registered new interface driver usbhid
[ 2.898212] usbhid: USB HID core driver
[ 2.902884] ashmem: initialized
[ 2.906228] logger: created 256K log 'log_main'
[ 2.910917] logger: created 256K log 'log_events'
[ 2.915792] logger: created 256K log 'log_radio'
[ 2.920569] logger: created 256K log 'log_system'
[ 2.926096] usbcore: registered new interface driver snd-usb-audio
[ 2.933730] fsl-asrc 2034000.asrc: driver registered
[ 3.003603] VT1613 SoC Audio Codec [ID = 5649 - 4123]
[ 3.011667] imx-ac97-vt1613 sound.18: vt1613-hifi-analog <-> 2028000.ssi mapping ok
[ 3.023525] imx-audio-hdmi sound-hdmi.19: hdmi-hifi <-> hdmi_audio.3 mapping ok
[ 3.031643] NET: Registered protocol family 26
[ 3.036121] u32 classifier
[ 3.038836] Actions configured
[ 3.042246] Netfilter messages via NETLINK v0.30.
[ 3.047041] nf_conntrack version 0.5.0 (16046 buckets, 64184 max)
[ 3.053675] ctnetlink v0.93: registering with nfnetlink.
[ 3.059476] xt_time: kernel timezone is -0000
[ 3.064160] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.069645] arp_tables: (C) 2002 David S. Miller
[ 3.074336] TCP: cubic registered
[ 3.077660] Initializing XFRM netlink socket
[ 3.082391] NET: Registered protocol family 10
[ 3.087874] mip6: Mobile IPv6
[ 3.090882] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 3.096493] sit: IPv6 over IPv4 tunneling driver
[ 3.101737] NET: Registered protocol family 17
[ 3.106234] NET: Registered protocol family 15
[ 3.110687] can: controller area network core (rev 20120528 abi 9)
[ 3.116937] NET: Registered protocol family 29
[ 3.121390] can: raw protocol (rev 20120528)
[ 3.125681] can: broadcast manager protocol (rev 20120528 t)
[ 3.131355] can: netlink gateway (rev 20130117) max_hops=1
[ 3.137002] 8021q: 802.1Q VLAN Support v1.8
[ 3.141452] Key type dns_resolver registered
[ 3.145884] Bluetooth: RFCOMM TTY layer initialized
[ 3.150788] Bluetooth: RFCOMM socket layer initialized
[ 3.155965] Bluetooth: RFCOMM ver 1.11
[ 3.159816] usbcore: registered new interface driver btusb
[ 3.165388] usbcore: registered new interface driver cdc_wdm
[ 3.172613] ThumbEE CPU extension supported.
[ 3.177637] usb_otg_vbus: disabling
[ 3.181145] regulator-dummy: disabling
[ 3.185681] file system registered
[ 3.189902] using random self ethernet address
[ 3.194393] using random host ethernet address
[ 3.198920] Number of LUNs=8
[ 3.201811] Mass Storage Function, version: 2009/09/11
[ 3.206985] LUN: removable file: (no medium)
[ 3.211471] android_usb gadget: android_usb ready
[ 3.216419] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:05:55 UTC (355)
[ 3.233513] ALSA device list:
[ 3.236497] #0: vt1613-audio
[ 3.239556] #1: imx-hdmi-soc
[ 3.243193] Freeing unused kernel memory: 288K (c095a000 - c09a2000)
[ 3.252013] init: init started!
[ 3.257131] init: init second stage started!
[ 3.262021] init: waitpid failed: No child processes
[ 3.267190] init: property_set("ro.zygote", "zygote32") failed
[ 3.273255] init: (Loading properties from /default.prop took 0.01s.)
[ 3.281847] init: (Parsing /init.environ.rc took 0.00s.)
[ 3.287546] init: (Parsing /init.usb.rc took 0.00s.)
[ 3.293565] init: (Parsing init.freescale.usb.rc took 0.00s.)
[ 3.299407] init: (Parsing init.freescale.i.MX6Q.rc took 0.00s.)
[ 3.305616] init: (Parsing init.bluetooth.rc took 0.00s.)
[ 3.311041] init: (Parsing /init.freescale.rc took 0.02s.)
[ 3.317077] init: (Parsing /init.usb.configfs.rc took 0.00s.)
[ 3.322928] init: (Parsing /init.zygote32.rc took 0.00s.)
[ 3.328505] init: (Parsing /init.trace.rc took 0.00s.)
[ 3.333680] init: (Parsing /init.rc took 0.05s.)
[ 3.338477] init: Starting service 'ueventd'...
[ 3.343584] init: Waiting for /dev/.coldboot_done...
[ 3.345317] ueventd: ueventd started!
[ 3.433611] ueventd: Coldboot took 0.09s.
[ 3.443116] init: Waiting for /dev/.coldboot_done took 0.10s.
[ 3.451251] init: write_file: Unable to open '/proc/sys/kernel/hung_task_timeout_secs': No such file or directory
[ 3.461646] init: write_file: Unable to open '/proc/sys/kernel/sched_tunable_scaling': No such file or directory
[ 3.471984] init: write_file: Unable to open '/proc/sys/kernel/sched_latency_ns': No such file or directory
[ 3.481790] init: write_file: Unable to open '/proc/sys/kernel/sched_wakeup_granularity_ns': No such file or directory
[ 3.492540] init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory
[ 3.503322] init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
[ 3.513109] init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
[ 3.521692] init: Starting service 'watchdogd'...
[ 3.527239] Console: switching to colour dummy device 80x30
[ 3.528696] watchdogd: watchdogd started (interval 10, margin 20)!
[ 3.563205] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: barrier=1
[ 3.571685] fs_mgr: __mount(source=/dev/block/mmcblk0p5,target=/system,type=ext4)=0
[ 3.580559] EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option
[ 3.594543] JBD2: recovery failed
[ 3.597940] EXT4-fs (mmcblk0p4): error loading journal
[ 3.604704] fs_mgr: __mount(source=/dev/block/mmcblk0p4,target=/data,type=ext4)=-1
[ 3.614124] fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk0p4 for mount /data type ext4 )
[ 3.626235] EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option
[ 3.639178] JBD2: recovery failed
[ 3.642575] EXT4-fs (mmcblk0p6): error loading journal
[ 3.649337] fs_mgr: __mount(source=/dev/block/mmcblk0p6,target=/cache,type=ext4)=-1
[ 3.659317] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p6 at /cache options: nomblk_io_submit error: Invalid argument
[ 3.677860] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
[ 3.686026] fs_mgr: __mount(source=/dev/block/mmcblk0p7,target=/device,type=ext4)=0
[ 3.693815] init: fs_mgr_mount_all returned an error
[ 3.699009] init: fs_mgr_mount_all returned unexpected error 255
[ 3.708275] init: Starting service 'logd'...
[ 3.912655] random: mkswap urandom read with 29 bits of entropy available
[ 3.918057] logd.auditd: start
[ 3.918093] logd.klogd: 3914816666
[ 3.927042] Adding 307196k swap on /dev/block/zram0. Priority:-1 extents:1 across:307196k SS
[ 3.947568] init: (Loading properties from /system/build.prop took 0.01s.)
[ 3.954566] init: (Loading properties from /vendor/build.prop took 0.00s.)
[ 3.961503] init: (Loading properties from /factory/factory.prop took 0.00s.)
[ 3.971179] init: Starting service 'vold'...
[ 3.976115] init: Not bootcharting.
[ 3.981172] init: Failed to reload policy
[ 3.985534] init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...
[ 4.013159] init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 186) exited with status 0
[ 4.022138] init: (Loading properties from /data/local.prop took 0.00s.)
[ 4.029015] init: Starting service 'logd-reinit'...
[ 4.037190] init: Starting service 'healthd'...
[ 4.042284] init: Starting service 'console'...
[ 4.045552] binder: 192:192 transaction failed 29189, size 0-0
>ù›[ 4.054696] init: Starting service 'servicemanager'...
[ 4.060475] init: Starting service 'surfaceflinger'...
[ 4.060502] logd.daemon: reinit
[ 4.104520] init: Starting service 'daemonsu'...
[ 4.109750] init: Service 'logd-reinit' (pid 189) exited with status 0
[ 4.116897] init: Starting service 'exec 1 (/system/bin/fakerclocal)'...
root@udoo_6dq:/ # [ 4.156899] warning: `daemonsu' uses 32-bit capabilities (legacy support in use)
[ 4.167149] init: Service 'daemonsu' (pid 211) exited with status 0
[ 4.349582] init: Service 'exec 1 (/system/bin/fakerclocal)' (pid 217) exited with status 0
[ 4.387282] cfg80211: Calling CRDA to update world regulatory domain
[ 4.393855] cfg80211: World regulatory domain updated:
[ 4.399005] cfg80211: DFS Master region: unset
[ 4.403392] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[ 4.413153] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[ 4.421205] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[ 4.430626] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[ 4.438711] cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[ 4.448250] cfg80211: (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[ 4.457768] cfg80211: (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[ 4.465921] cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[ 4.473977] cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[ 4.518079] init: property_set("ro.ril.wake_lock_timeout", "300") failed
[ 4.525553] init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
[ 4.534839] init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
[ 4.545167] init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
[ 4.556188] init: Starting service 'disableadk'...
[ 4.578073] init: Service 'disableadk' (pid 248) exited with status 0
[ 5.046695] healthd: No charger supplies found
[ 5.051210] healthd: No battery devices found
[ 5.302461] init: Starting service 'bootanim'...
[ 9.076787] random: nonblocking pool is initialized
[ 16.085963] usb 1-1.1: USB disconnect, device number 3
random: nonblocking pool is initialized
/system/bin/sh: random:: not found
127|root@udoo_6dq:/ #
127|root@udoo_6dq:/ # reboot
[ 92.092267] imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!
[ 92.098742] reboot: Restarting system with command ''
U-Boot SPL 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)
SPL: u-boot second stage will be loaded from MMC0
U-Boot 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 40 C
Reset cause: WDOG
Board: UDOO Quad
Watchdog enabled
DRAM: 1 GiB
MMC: FSL_SDHC: 0
*** Warning - bad CRC, using default environment
auto-detected panel HDMI
Display: HDMI (1280x720)
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:0
Net: using phy at 6
FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 3 2 1 0
112 bytes read in 148 ms (0 Bytes/s)
Running bootscript from mmc ...
Device Tree: dts/imx6q-udoo-hdmi.dtb
42833 bytes read in 86 ms (486.3 KiB/s)
boota mmc0
kernel @ 14008000 (5719992)
ramdisk @ 15000000 (917604)
fdt @ 14f00000 (42833)
## Booting Android Image at 0x12000000 ...
Kernel load addr 0x14008000 size 5586 KiB
Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
Loading Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f0d750
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 3.14.52-09424-g6fe6e7b-dirty (root@eyenai-VirtualBox) (gcc version 5.3.1 20160401 (optimized) (UBERTC-5.3.x) ) #1 SMP PREEMPT Wed Feb 7 21:19:47 CET 2018
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: UDOO Quad Board
[ 0.000000] cma: CMA: reserved 256 MiB at 2e000000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] PERCPU: Embedded 8 pages/cpu @ee741000 s8640 r8192 d15936 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260384
[ 0.000000] Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend androidboot.serialno=0c09a1d4e3173fe7
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 763932K/1047552K available (7132K kernel code, 439K rwdata, 2408K rodata, 288K init, 497K bss, 283620K reserved, 277504K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xef800000 - 0xff000000 ( 248 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef000000 ( 752 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0959514 (9542 kB)
[ 0.000000] .init : 0xc095a000 - 0xc09a21c0 ( 289 kB)
[ 0.000000] .data : 0xc09a4000 - 0xc0a11d80 ( 440 kB)
[ 0.000000] .bss : 0xc0a11d8c - 0xc0a8e400 ( 498 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] L310 cache controller enabled
[ 0.000000] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB
[ 0.000000] Switching to timer-based delay loop
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
[ 0.000815] Console: colour dummy device 80x30
[ 0.000838] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.000851] pid_max: default: 32768 minimum: 301
[ 0.000957] Security Framework initialized
[ 0.001011] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001024] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001670] Initializing cgroup subsys debug
[ 0.001683] Initializing cgroup subsys freezer
[ 0.001709] CPU: Testing write buffer coherency: ok
[ 0.001958] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002010] Setting up static identity map for 0x106cebc0 - 0x106cec18
[ 0.061004] CPU1: Booted secondary processor
[ 0.061023] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080987] CPU2: Booted secondary processor
[ 0.081007] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.100988] CPU3: Booted secondary processor
[ 0.101009] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.101111] Brought up 4 CPUs
[ 0.101139] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[ 0.101148] CPU: All CPU(s) started in SVC mode.
[ 0.101580] devtmpfs: initialized
[ 0.105169] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.105495] pinctrl core: initialized pinctrl subsystem
[ 0.105799] regulator-dummy: no parameters
[ 0.119914] NET: Registered protocol family 16
[ 0.127808] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.128353] cpuidle: using governor ladder
[ 0.128363] cpuidle: using governor menu
[ 0.128756] CPU identified as i.MX6Q, silicon rev 1.2
[ 0.128878] Use WDOG1 as reset source
[ 0.135781] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
[ 0.136056] vdd1p1: 800 <--> 1375 mV at 1100 mV
[ 0.136379] vdd3p0: 2625 <--> 3400 mV at 3000 mV
[ 0.136690] vdd2p5: 2000 <--> 2750 mV at 2400 mV
[ 0.136988] vddarm: 725 <--> 1450 mV at 1150 mV
[ 0.140366] vddpu: 725 <--> 1450 mV
[ 0.140694] vddsoc: 725 <--> 1450 mV at 1175 mV
[ 0.142480] syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
[ 0.144581] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
[ 0.147971] apx_wdog trigger loaded
[ 0.147990] apx_wdog: enabled wdog - 0 s between refresh
[ 0.148866] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.148877] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.149512] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.170992] bio: create slab <bio-0> at 0
[ 0.172866] mxs-dma 110000.dma-apbh: initialized
[ 0.173469] usb_h1_vbus: 5000 mV
[ 0.173660] usb_otg_vbus: 5000 mV
[ 0.173848] 2P5V: 2500 mV
[ 0.174187] i2c-core: driver [max17135] using legacy suspend method
[ 0.174196] i2c-core: driver [max17135] using legacy resume method
[ 0.174718] SCSI subsystem initialized
[ 0.175147] usbcore: registered new interface driver usbfs
[ 0.175208] usbcore: registered new interface driver hub
[ 0.175303] usbcore: registered new device driver usb
[ 0.175428] usbphy_nop1.11 supply vcc not found, using dummy regulator
[ 0.175519] usbphy_nop2.12 supply vcc not found, using dummy regulator
[ 0.176647] i2c i2c-1: IMX I2C adapter registered
[ 0.177443] i2c i2c-2: IMX I2C adapter registered
[ 0.177553] Linux video capture interface: v2.00
[ 0.177599] pps_core: LinuxPPS API ver. 1 registered
[ 0.177608] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.177632] PTP clock support registered
[ 0.190414] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.210399] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.211453] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
[ 0.211469] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
[ 0.211532] MIPI CSI2 driver module loaded
[ 0.211609] Advanced Linux Sound Architecture Driver Initialized.
[ 0.212654] Loading modules backported from Linux version v4.1.7-0-g0c5c1f1
[ 0.212663] Backport integrated by backports.git v4.1.1-1-0-g8286954
[ 0.212672] Bluetooth: Core ver 2.20
[ 0.212722] NET: Registered protocol family 31
[ 0.212730] Bluetooth: HCI device and connection manager initialized
[ 0.212745] Bluetooth: HCI socket layer initialized
[ 0.212758] Bluetooth: L2CAP socket layer initialized
[ 0.212792] Bluetooth: SCO socket layer initialized
[ 0.213223] Switched to clocksource mxc_timer1
[ 0.222282] NET: Registered protocol family 2
[ 0.223093] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.223175] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.223325] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.223402] TCP: reno registered
[ 0.223417] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.223458] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.223698] NET: Registered protocol family 1
[ 0.223925] Trying to unpack rootfs image as initramfs...
[ 0.277176] Freeing initrd memory: 896K (c5000000 - c50e0000)
[ 0.277788] hw perfevents: enabled with ARMv7_Cortex_A9 PMU driver, 7 counters available
[ 0.278545] imx_busfreq busfreq.15: DDR medium rate not supported.
[ 0.278984] Bus freq driver module loaded
[ 0.280168] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.281735] bounce pool size: 64 pages
[ 0.286901] VFS: Disk quotas dquot_6.5.2
[ 0.287140] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.288476] NTFS driver 2.1.30 [Flags: R/W].
[ 0.288911] fuse init (API version 7.22)
[ 0.289311] msgmni has been set to 1463
[ 0.292122] NET: Registered protocol family 38
[ 0.292162] io scheduler noop registered
[ 0.292172] io scheduler deadline registered
[ 0.292206] io scheduler cfq registered (default)
[ 0.292633] imx-weim 21b8000.weim: Driver registered.
[ 0.294122] MIPI DSI driver module loaded
[ 0.295159] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[ 0.295188] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[ 0.295275] mxc_sdc_fb fb.20: registered mxc display driver hdmi
[ 0.333301] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 0.402818] Console: switching to colour frame buffer device 240x67
[ 0.442875] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[ 0.443428] imx-sdma 20ec000.sdma: no event needs to be remapped
[ 0.443877] imx-sdma 20ec000.sdma: loaded firmware 3.3
[ 0.446381] imx-sdma 20ec000.sdma: initialized
[ 0.446791] Serial: IMX driver
[ 0.447151] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
[ 1.294894] console [ttymxc1] enabled
[ 1.295296] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
[ 1.295584] serial: Freescale lpuart driver
[ 1.296578] [drm] Initialized drm 1.1.0 20060810
[ 1.296947] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[ 1.303808] brd: module loaded
[ 1.307487] loop: module loaded
[ 1.307952] zram: Created 1 device(s) ...
[ 1.308294] [bossac] Registering IRQ 323 for BOSSAC Arduino erase/reset operation
[ 1.308516] [bossac] Created device file /dev/udoo_ard
[ 1.309364] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[ 1.309372] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[ 1.309379] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[ 1.309385] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[ 1.313032] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[ 1.313061] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 1.313073] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 1.314776] scsi0 : ahci_platform
[ 1.315038] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
[ 1.317124] tun: Universal TUN/TAP device driver, 1.6
[ 1.317127] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 1.317292] CAN device driver interface
[ 1.318206] 2188000.ethernet supply phy not found, using dummy regulator
[ 1.433600] pps pps0: new PPS source ptp0
[ 1.479252] libphy: fec_enet_mii_bus: probed
[ 1.479717] fec 2188000.ethernet eth0: registered PHC device 0
[ 1.479905] PPP generic driver version 2.4.2
[ 1.480091] PPP BSD Compression module registered
[ 1.480094] PPP Deflate Compression module registered
[ 1.480116] PPP MPPE Compression module registered
[ 1.480121] NET: Registered protocol family 24
[ 1.480194] usbcore: registered new interface driver asix
[ 1.480249] usbcore: registered new interface driver ax88179_178a
[ 1.480288] usbcore: registered new interface driver cdc_ether
[ 1.480325] usbcore: registered new interface driver cdc_eem
[ 1.480363] usbcore: registered new interface driver net1080
[ 1.480401] usbcore: registered new interface driver cdc_subset
[ 1.480437] usbcore: registered new interface driver zaurus
[ 1.480514] usbcore: registered new interface driver cdc_ncm
[ 1.480518] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.480521] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 1.480660] usbcore: registered new interface driver cdc_acm
[ 1.480662] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.480719] usbcore: registered new interface driver usb-storage
[ 1.480819] usbcore: registered new interface driver usbserial
[ 1.480860] usbcore: registered new interface driver usbserial_generic
[ 1.480894] usbserial: USB Serial support registered for generic
[ 1.480929] usbcore: registered new interface driver ftdi_sio
[ 1.480962] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.481002] usbcore: registered new interface driver option
[ 1.481034] usbserial: USB Serial support registered for GSM modem (1-port)
[ 1.481076] usbcore: registered new interface driver usb_ehset_test
[ 1.481812] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 1.489791] ci_hdrc ci_hdrc.1: doesn't support gadget
[ 1.489809] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 1.489834] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[ 1.503290] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 1.503459] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.503468] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.503474] usb usb1: Product: EHCI Host Controller
[ 1.503479] usb usb1: Manufacturer: Linux 3.14.52-09424-g6fe6e7b-dirty ehci_hcd
[ 1.503485] usb usb1: SerialNumber: ci_hdrc.1
[ 1.504077] hub 1-0:1.0: USB hub found
[ 1.504110] hub 1-0:1.0: 1 port detected
[ 1.505006] mousedev: PS/2 mouse device common for all mice
[ 1.505469] usbcore: registered new interface driver usbtouchscreen
[ 1.505945] input: st1232-touchscreen as /devices/soc0/soc.0/2100000.aips-bus/21a8000.i2c/i2c-2/2-0055/input/input0
[ 1.506776] snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
[ 1.507057] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
[ 1.507150] i2c /dev entries driver
[ 1.508263] 2-003c supply DOVDD not found, using dummy regulator
[ 1.508321] 2-003c supply DVDD not found, using dummy regulator
[ 1.508357] 2-003c supply AVDD not found, using dummy regulator
[ 1.663409] ata1: SATA link down (SStatus 0 SControl 300)
[ 1.663449] ahci-imx 2200000.sata: no device found, disabling link.
[ 1.663455] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[ 1.698228] ov5640_read_reg:write reg error:reg=300a
[ 1.698230] camera ov5640_mipi is not found
[ 1.698986] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video16
[ 1.699113] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video17
[ 1.699381] usbcore: registered new interface driver uvcvideo
[ 1.699383] USB Video Class driver (1.1.1)
[ 1.699628] [UDOO power-off] Probed LVDS power.
[ 1.699709] [UDOO power-off] Probed LVDS backlight.
[ 1.699777] [UDOO power-off] Probed UDOO Quad/Dual.
[ 1.700170] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
[ 1.700487] device-mapper: uevent: version 1.0.3
[ 1.700808] device-mapper: ioctl: 4.27.0-ioctl (2013-10-30) initialised: dm-devel@redhat.com
[ 1.701182] sdhci: Secure Digital Host Controller Interface driver
[ 1.701184] sdhci: Copyright(c) Pierre Ossman
[ 1.701187] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.706530] mmc0: no vqmmc regulator found
[ 1.706536] mmc0: no vmmc regulator found
[ 1.743251] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[ 1.743904] Warning: No contiguous memory is reserverd for gpu.!
[ 1.743904]
[ 1.743910] Warning: Will use default value(134217728) for the reserved memory!
[ 1.743910]
[ 1.743915] Galcore version 5.0.11.41671
[ 1.843372] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 1.937342] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.955177] mmc0: new high speed SDHC card at address 0007
[ 1.955877] mmcblk0: mmc0:0007 SD32G 29.0 GiB
[ 1.990075] mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
[ 2.042141] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[ 2.042150] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.048796] hub 1-1:1.0: USB hub found
[ 2.056750] hub 1-1:1.0: 4 ports detected
[ 2.256969] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 2.257492] mxc_vpu 2040000.vpu: VPU initialized
[ 2.373516] usb 1-1.3: new high-speed USB device number 3 using ci_hdrc
[ 2.503521] caam 2100000.caam: Instantiated RNG4 SH0
[ 2.521267] usb 1-1.3: New USB device found, idVendor=148f, idProduct=5370
[ 2.528169] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 2.535534] usb 1-1.3: Product: 802.11 n WLAN
[ 2.539901] usb 1-1.3: Manufacturer: Ralink
[ 2.544107] usb 1-1.3: SerialNumber: 1.0
[ 2.748725] caam 2100000.caam: Instantiated RNG4 SH1
[ 2.753720] caam 2100000.caam: device ID = 0x0a160100 (Era 4)
[ 2.759477] caam 2100000.caam: job rings = 2, qi = 0
[ 2.826143] caam algorithms registered in /proc/crypto
[ 2.834941] caam_jr 2101000.jr0: registering rng-caam
[ 2.840811] snvs-secvio 20cc000.caam-snvs: can't get snvs clock
[ 2.846782] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
[ 2.855086] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.862822] usbcore: registered new interface driver usbhid
[ 2.868446] usbhid: USB HID core driver
[ 2.873031] ashmem: initialized
[ 2.876387] logger: created 256K log 'log_main'
[ 2.881078] logger: created 256K log 'log_events'
[ 2.885964] logger: created 256K log 'log_radio'
[ 2.890743] logger: created 256K log 'log_system'
[ 2.896255] usbcore: registered new interface driver snd-usb-audio
[ 2.903878] fsl-asrc 2034000.asrc: driver registered
[ 2.973557] VT1613 SoC Audio Codec [ID = 5649 - 4123]
[ 2.981651] imx-ac97-vt1613 sound.18: vt1613-hifi-analog <-> 2028000.ssi mapping ok
[ 2.993550] imx-audio-hdmi sound-hdmi.19: hdmi-hifi <-> hdmi_audio.3 mapping ok
[ 3.001688] NET: Registered protocol family 26
[ 3.006175] u32 classifier
[ 3.008890] Actions configured
[ 3.012300] Netfilter messages via NETLINK v0.30.
[ 3.017093] nf_conntrack version 0.5.0 (16046 buckets, 64184 max)
[ 3.023745] ctnetlink v0.93: registering with nfnetlink.
[ 3.029601] xt_time: kernel timezone is -0000
[ 3.034292] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.039768] arp_tables: (C) 2002 David S. Miller
[ 3.044465] TCP: cubic registered
[ 3.047789] Initializing XFRM netlink socket
[ 3.052514] NET: Registered protocol family 10
[ 3.057978] mip6: Mobile IPv6
[ 3.060985] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 3.066610] sit: IPv6 over IPv4 tunneling driver
[ 3.071846] NET: Registered protocol family 17
[ 3.076344] NET: Registered protocol family 15
[ 3.080797] can: controller area network core (rev 20120528 abi 9)
[ 3.087051] NET: Registered protocol family 29
[ 3.091505] can: raw protocol (rev 20120528)
[ 3.095796] can: broadcast manager protocol (rev 20120528 t)
[ 3.101469] can: netlink gateway (rev 20130117) max_hops=1
[ 3.107118] 8021q: 802.1Q VLAN Support v1.8
[ 3.111547] Key type dns_resolver registered
[ 3.115991] Bluetooth: RFCOMM TTY layer initialized
[ 3.120894] Bluetooth: RFCOMM socket layer initialized
[ 3.126076] Bluetooth: RFCOMM ver 1.11
[ 3.129925] usbcore: registered new interface driver btusb
[ 3.135501] usbcore: registered new interface driver cdc_wdm
[ 3.142719] ThumbEE CPU extension supported.
[ 3.147741] usb_otg_vbus: disabling
[ 3.151249] regulator-dummy: disabling
[ 3.155558] file system registered
[ 3.159742] using random self ethernet address
[ 3.164238] using random host ethernet address
[ 3.168764] Number of LUNs=8
[ 3.171654] Mass Storage Function, version: 2009/09/11
[ 3.176820] LUN: removable file: (no medium)
[ 3.181319] android_usb gadget: android_usb ready
[ 3.186276] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:07:33 UTC (453)
[ 3.203341] ALSA device list:
[ 3.206330] #0: vt1613-audio
[ 3.209404] #1: imx-hdmi-soc
[ 3.213045] Freeing unused kernel memory: 288K (c095a000 - c09a2000)
[ 3.221809] init: init started!
[ 3.226896] init: init second stage started!
[ 3.231791] init: waitpid failed: No child processes
[ 3.236964] init: property_set("ro.zygote", "zygote32") failed
[ 3.243020] init: (Loading properties from /default.prop took 0.01s.)
[ 3.251620] init: (Parsing /init.environ.rc took 0.00s.)
[ 3.257357] init: (Parsing /init.usb.rc took 0.00s.)
[ 3.263374] init: (Parsing init.freescale.usb.rc took 0.00s.)
[ 3.269217] init: (Parsing init.freescale.i.MX6Q.rc took 0.00s.)
[ 3.275383] init: (Parsing init.bluetooth.rc took 0.00s.)
[ 3.280805] init: (Parsing /init.freescale.rc took 0.02s.)
[ 3.286872] init: (Parsing /init.usb.configfs.rc took 0.00s.)
[ 3.292724] init: (Parsing /init.zygote32.rc took 0.00s.)
[ 3.298285] init: (Parsing /init.trace.rc took 0.00s.)
[ 3.303477] init: (Parsing /init.rc took 0.05s.)
[ 3.308291] init: Starting service 'ueventd'...
[ 3.313405] init: Waiting for /dev/.coldboot_done...
[ 3.315134] ueventd: ueventd started!
[ 3.401670] uåÑ›Ù_œá«V“ú[ 3.406169] init: write_file: Unable to open '/proc/sys/kernel/hung_task_timeout_secs': No such file or directory
[ 3.416617] init: write_file: Unable to open '/proc/sys/kernel/sched_tunable_scaling': No such file or directory
[ 3.426887] init: write_file: Unable to open '/proc/sys/kernel/sched_latency_ns': No such file or directory
[ 3.436701] init: write_file: Unable to open '/proc/sys/kernel/sched_wakeup_granularity_ns': No such file or directory
[ 3.447469] init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory
[ 3.458259] init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
[ 3.468081] init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
[ 3.476668] init: Starting service 'watchdogd'...
[ 3.482165] Console: switching to colour dummy device 80x30
[ 3.489233] watchdogd: watchdogd started (interval 10, margin 20)!
[ 3.512908] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: barrier=1
[ 3.521369] fs_mgr: __mount(source=/dev/block/mmcblk0p5,target=/system,type=ext4)=0
[ 3.530216] EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option
[ 3.544467] JBD2: recovery failed
[ 3.547800] EXT4-fs (mmcblk0p4): error loading journal
[ 3.553173] fs_mgr: __mount(source=/dev/block/mmcblk0p4,target=/data,type=ext4)=-1
[ 3.562594] fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk0p4 for mount /data type ext4 )
[ 3.574705] EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option
[ 3.588424] JBD2: recovery failed
[ 3.591752] EXT4-fs (mmcblk0p6): error loading journal
[ 3.597132] fs_mgr: __mount(source=/dev/block/mmcblk0p6,target=/cache,type=ext4)=-1
[ 3.607110] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p6 at /cache options: nomblk_io_submit error: Invalid argument
[ 3.624964] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
[ 3.633095] fs_mgr: __mount(source=/dev/block/mmcblk0p7,target=/device,type=ext4)=0
[ 3.640885] init: fs_mgr_mount_all returned an error
[ 3.646115] init: fs_mgr_mount_all returned unexpected error 255
[ 3.655366] init: Starting service 'logd'...
[ 3.854781] random: mkswap urandom read with 30 bits of entropy available
[ 3.864217] Adding 307196k swap on /dev/block/zram0. Priority:-1 extents:1 across:307196k SS
[ 3.894278] init: (Loading properties from /system/build.prop took 0.02s.)
[ 3.901321] init: (Loading properties from /vendor/build.prop took 0.00s.)
[ 3.908696] init: (Loading properties from /factory/factory.prop took 0.00s.)
[ 3.918508] init: Starting service 'vold'...
[ 3.922730] logd.auditd: start
[ 3.922767] logd.klogd: 3919536666
[ 3.930236] init: Not bootcharting.
[ 3.935322] init: Failed to reload policy
[ 3.939661] init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...
[ 3.971229] init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 184) exited with status 0
[ 3.980136] init: (Loading properties from /data/local.prop took 0.00s.)
[ 3.986993] init: Starting service 'logd-reinit'...
[ 3.995242] init: Starting service 'healthd'...
[ 4.000308] init: Starting service 'console'...
[ 4.003215] binder: 193:193 transaction failed 29189, size 0-0
At¨ >ù›[ 4.012601] init: Starting service 'servicemanager'...
[ 4.018383] init: Starting service 'surfaceflinger'...
[ 4.030002] init: Starting service 'daemonsu'...
[ 4.030317] logd.daemon: reinit
[ 4.038689] init: Service 'logd-reinit' (pid 190) exited with status 0
[ 4.046153] init: Starting service 'exec 1 (/system/bin/fakerclocal)'...
[ 4.091215] warning: `daemonsu' uses 32-bit capabilities (legacy support in use)
root@udoo_6dq:/ # [ 4.101010] init: Service 'daemonsu' (pid 208) exited with status 0
[ 4.248258] init: Service 'exec 1 (/system/bin/fakerclocal)' (pid 212) exited with status 0
[ 4.283738] cfg80211: Calling CRDA to update world regulatory domain
[ 4.290284] cfg80211: World regulatory domain updated:
[ 4.295496] cfg80211: DFS Master region: unset
[ 4.299862] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[ 4.309900] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[ 4.317950] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[ 4.327389] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[ 4.335434] cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[ 4.345010] cfg80211: (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[ 4.354568] cfg80211: (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[ 4.362680] cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[ 4.370711] cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[ 4.416839] init: property_set("ro.ril.wake_lock_timeout", "300") failed
[ 4.424510] init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
[ 4.433856] init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
[ 4.444211] init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
[ 4.455180] init: Starting service 'disableadk'...
[ 4.492947] init: Service 'disableadk' (pid 248) exited with status 0
[ 5.004352] healthd: No charger supplies found
[ 5.004381] healthd: No battery devices found
[ 5.256877] init: Starting service 'bootanim'...
[ 9.280707] random: nonblocking pool is initialized
Hi Julian
what bsp used in the case, one can try with nxp android releases described on
In general for reliable reboot it is necessary to shortly remove power fom all board
using pmic pwron signal as in spf-27392 i.MX6Q Sabre SD schematic p.21.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have the same issue if a shutdown or unplugged directly, this is a udoo board, and if I flash the sdcard with his android image doesn't occur, but if i compile their android i have this issue