S32K v3.0.0 and R2017b license error solved

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K v3.0.0 and R2017b license error solved

786 Views
lethuer2
Contributor II

Hello dumitru-daniel.popa

first time I have a tipp for you !

Like discussed here https://community.nxp.com/thread/467938#comment-980540 I wanted to use S32Kv3.0.0 toolbox with R2017b and got this license error:

Unbenannt.PNG

I made all the steps recommended and completely new downloaded and installed the toolbox.

- I generated a new license file and saved it with the file extension .lic to the installation folder

RESET the MATLAB default paths to DEFAULT using the Set Path menu to remove all previous toolboxes

- run the mbd_s32K_path.m to add the S32K1xx into MATLAB

added the lic folder manually to the Matlab paths

In opposite to v2.0 (which does not work with R2017b) I was not able to change the path during installation of v3.0.

So now I simply copied the installed content of v3.0 toolbox from the automatic generated path to a different folder and that solved the problem after simply running the mbd_s32K_path.m again.

Maybe the standard installation path was too long or the space in my username leads to some problems so the lic file couldn't be found. 

Anyway...

Best regards

Leon

0 Kudos
1 Reply

598 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi Leon, 

Thank you for reporting this and glad to find out you have resolved.

You can change the default Add-Ons installation paths directly from MATLAB Preferences before Toolbox install.

pastedImage_1.png

Best regards,

Daniel

0 Kudos