IMX6DQ DDR3 stress test failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DQ DDR3 stress test failure

Jump to solution
764 Views
wyb0116
Contributor II

I meet a problem that is ddr3 stress test failure like below

always failure at 64bit 's MSB 32bit write vlaue error

ddr3 test script is "MX6Q_ARD_DDR3_register_programming_aid_v1.5.inc "

============================================ 
DDR Stress Test (2.6.0) 
Build: Aug 1 2017, 17:33:25 
NXP Semiconductors. 
============================================ 

============================================ 
Chip ID 
CHIP ID = i.MX6 Dual/Quad (0x63) 
Internal Revision = TO1.2 
============================================ 

============================================ 
Boot Configuration 
SRC_SBMR1(0x020d8004) = 0x00021040 
SRC_SBMR2(0x020d801c) = 0x12000001 
============================================ 

ARM Clock set to 1GHz 

============================================ 
DDR configuration 
BOOT_CFG3[5-4]: 0x00, Single DDR channel. 
DDR type is DDR3 
Data width: 64, bank num: 8 
Row size: 15, col size: 10 
Chip select CSD0 is used 
Density per chip select: 2048MB 
============================================ 


DDR Stress Test Iteration 1 
Current Temperature: 46 
============================================ 

DDR Freq: 528 MHz 
t0.1: data is addr test 
t0: memcpy10 SSN x64 test 
Address of bank1 failure: 0x2182fec0 
Data initially read was: 0xFFFFFEC4FFFFFFFF 
Data re-read is: 0xFFFFFEC4FFFFFFFF 
But pattern was: 0xFFFFFFFFFFFFFFFF 
Error: failed to run stress test!!! 


0x0 0x4 0x8 0xC 
---------------------------------------------------------------------------------------------------------------- 
0x2182FEC0: 0xFFFFFFFF 0xFFFFFEC4 0x00001000 0x0000FECC 
0x2182FED0: 0xFFFFFFFF 0xFFFFFED4 0x00002000 0x0000FEDC 
0x2182FEE0: 0xFFFFFFFF 0xFFFFFEE4 0x00004000 0x0000FEEC 
0x2182FEF0: 0xFFFFFFFF 0xFFFFFEF4 0x00008000 0x0000FEFC 
0x2182FF00: 0xFFFFFFFF 0xFFFFFFFF 0x00010000 0x00000000 
0x2182FF10: 0xFFFFFFFF 0xFFFFFFFF 0x00020000 0x00000000 
0x2182FF20: 0xFFFFFFFF 0xFFFFFFFF 0x00040000 0x00000000 
0x2182FF30: 0xFFFFFFFF 0xFFFFFFFF 0x00080000 0x00000000 
memory read is done 

Hardware:

My design reference the sabre sdb 1GB ddr3 board。

ONLY change the ddr3 part number to fit the 2GB。“MT41K128M16JT-125 ” to “MT41K256M16HA-125IT”

The ddr3‘s signal route was same with the sabre sdb board 。

The sabre sdb use 8 layer layout, but I use 6 layer board layout to cost down and the DDR_VREF voltage use lines not plane。

无标题.jpg

Is this layout was poor,have any suggestion for me?

Can I fix this “ddr3’s stress test failure” problem by change the MMDC regs value?

or change the poor layout first?

Have any success IMX6DQ design use the 6 layers board before? 

Labels (2)
0 Kudos
1 Solution
545 Views
igorpadykov
NXP Employee
NXP Employee

Hi yibo

such kind of errors may point to layout errors: broken or

connected together signal lines, one can check signals (in red) with

oscilloscope writing/reading problematic bit patterns with jtag.

May be recommended to recheck i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
546 Views
igorpadykov
NXP Employee
NXP Employee

Hi yibo

such kind of errors may point to layout errors: broken or

connected together signal lines, one can check signals (in red) with

oscilloscope writing/reading problematic bit patterns with jtag.

May be recommended to recheck i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
545 Views
wyb0116
Contributor II

But i am confusing with that the  "data is addr test" was passed in stress testing. Is that can prove the hardware connection was right?

The value in red like  addr that is the “data is addr test” step leave.

thanks for you reply. :smileyhappy:

0 Kudos