Hi -
We have a custom board running a i.MX6ULL with 512MB DDR3. We are running the "DDR Stress Test (2.6.0)" tool from NXP....we are using the GUI version over USB. My question is: Now that I have the calibration factors generated by the tool, where do I apply them to Uboot/Linux? We are running the uboot-rel_imx_4.9.x_1.0.0_ga and linux-rel_imx_4.9.x for Uboot and Linux respectively. It seems to me like there should be a script file somewhere that should do this, but I cannot seem to find it in either of these packages. please help.
thanks in advance
Chad
Hi Chad
calibration coefficients may be added to uboot dcd header :
uboot/board/freescale/mx6ullevk/imximage.cfg
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor-
I actually found this about an hour after I posted the question. Happy to have it confirmed
Thanks
Chad
Sent from my iPhone