AnsweredAssumed Answered

Bal Driver Implementation and timing

Question asked by sandeep bettahalli on Feb 15, 2018
Latest reply on Mar 19, 2018 by Martinez Garcia

Hi,

We are using PN5180 on Linux based custom board used for payment applications. 

Using example applications, we see that there are around 3 sec delay between some of the transactions.

We use Bal driver from https://github.com/NXPNFCLinux/nxprdlib-kernel-bal and SW3693-1 package from NXP as reader library.

One of the obvious problems I see with BAL driver is, it registers for only Falling edge of busy line.

status = request_threaded_irq(bal.busy_irq, bal_busy_isr,
NULL,
IRQF_TRIGGER_FALLING,
"bal", &bal);

For the first transaction, Bal_write will not wait for busy line and goes ahead and performs SPI write, but for next transaction, it will wait for 3 secs as the timeout for completion in bal_write is 3 secs. The only possible way to avoid this 3 seconds is, if data is fed continuously and PN5180 completes write/read transaction and brings down busy line in this 3 secs waiting time of next write/read.

 

Is this how it was designed?

Shouldn't driver hold the status of busy line by registering for both IRQF_TRIGGER_FALLING and IRQF_TRIGGER_RISING and read the busy line (as most likely it will be connected to GPIO) and keep track of busy line status. Go to wait in read/write only if busy line is high.

 

Regards,

Sandeep

Outcomes