AnsweredAssumed Answered

Motion Sequence Builder will not compile

Question asked by Michael Bray on Feb 14, 2018
Latest reply on Feb 15, 2018 by Michael Bray

When using the Motion Sequence Builder tool in the Kinetis Motor Suite, I am having trouble compiling the code. Everything works fine when I am working in sensored velocity, but when I am in sensored position it fails to compile. I looked through the log file, and its failing with it can't find the MotionSequence.h file. Which is odd because the related *.c file on the line above is called MotionSequencePos.c and there is a MotionSequencePos.h. I tried renaming MotionSequencePos.h to what the makefile was looking for, but the build still fails further down the line. Is there any reason why motion Sequence Builder just isn't working? I'm not doing anything complex.

Outcomes