Hello,
I am using LPC54102 and I am trying to run example code from LPCopen library. If I run example code as it is on may hardware it is working fine, but I if make changes in SSEL pin i.e Slave select pin it is not working as expected.
Please help me related same.
Thanks Victor, I'll try with SDK.
Tejal
Hello Tejal,
Are you using the example periph_spi_sm_int from the LPCopen or another one?
What pin are you selecting when you make the change for the Slave select pin?
The LPC54102 board has SDK, so I recommend you to use this instead of the LPCOpen, this because SDK is the newest software so all the new updates and bug fixes will come for SDK only. You can download it from here
I'll be waiting for your answer to continue with this problem!
Have a great day,
Victor.