I try to configure uboot to start from ocram. RM says, that OCRAM area starts from 0x0090 0000. In uboot config i add string:
#define CONFIG_SYS_TEXT_BASE 0x00908000
Then i build uboot, put device into recovery mode and try to update. At this stage i have error:
Colibri iMX7 rootfs detected
Put the module in recovery mode and press [ENTER]...
config file <imx_flash/imx_usb.conf>
vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf
vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf
vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf
vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x007d file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0076 file_name=mx7_usb_work.conf
vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf
vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf
vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf
vid=0x066f pid=0x37ff file_name=linux_gadget.conf
config file <imx_flash/mx7_usb_work.conf>
parse imx_flash/mx7_usb_work.conf
15a2:0076(mx7) bConfigurationValue =1
Interface 0 claimed
HAB security state: development mode (0x56787856)
== work item
filename colibri-imx7_bin/u-boot-nand.imx
load_size 0 bytes
load_addr 0x00000000
dcd 1
clear_dcd 0
plug 1
jump_mode 2
jump_addr 0x00000000
== end work item
main dcd length 1b4
sub dcd length 164
sub dcd length c
Check Data Command(10) success @307900c4=1c1 mask 1
sub dcd length 34
sub dcd length c
Check Data Command(10) success @307a0004=1 mask 1
loading binary file(colibri-imx7_bin/u-boot-nand.imx) to 00907000, skip=0, fsize=89000 type=aa
out err=-1, last_trans=0 cnt=0x3c00 max=0x400 transferSize=0x400 retry=0
out err=-4, last_trans=0 cnt=0x3c00 max=0x200 transferSize=0x400 retry=1
out err=-4, last_trans=0 cnt=0x3c00 max=0x100 transferSize=0x400 retry=2
out err=-4, last_trans=0 cnt=0x3c00 max=0x80 transferSize=0x400 retry=3
out err=-4, last_trans=0 cnt=0x3c00 max=0x40 transferSize=0x400 retry=4
out err=-4, last_trans=0 cnt=0x3c00 max=0x20 transferSize=0x400 retry=5
out err=-4, last_trans=0 cnt=0x3c00 max=0x10 transferSize=0x400 retry=6
out err=-4, last_trans=0 cnt=0x3c00 max=0x8 transferSize=0x400 retry=7
out err=-4, last_trans=0 cnt=0x3c00 max=0x10 transferSize=0x400 retry=8
out err=-4, last_trans=0 cnt=0x3c00 max=0x8 transferSize=0x400 retry=9
out err=-4, last_trans=0 cnt=0x3c00 max=0x10 transferSize=0x400 retry=10
Giving up
HAB security state: development mode (0x00000000)
I'm doing the right thing?
Hi Vladimir
seems this is specific board issue and may be posted on board vendor wiki
Welcome to - Toradex Community
or uboot mail list
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------