AnsweredAssumed Answered

no output in terminal with mbed serial (Window 10)

Question asked by Tuan Mai Employee on Feb 9, 2018
Latest reply on Apr 20, 2018 by Tuan Mai

I am using Window 10.  When connecting the LS1043ARDB mbed Serial Port (COM7) - which can be seen by TeraTerm.  I set baud rate to 1152000,8, no parity, 1 stop bit and none flow control (normal setting) but I do not see any output to the terminal.  I did also try with Putty with the same setting and the result is the same (no output).  I tried the LS1043ARDB with my Ubuntu machine with minicom and I can see the uboot output - This is to make sure the LS1043ARDB is functional -  Any idea why I do not see output in Window 10

Outcomes