iMX6Q - sabresd cusomised board , the panel type model is KD101N70-40NV-A002, this panel has Support in Linux or Not ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q - sabresd cusomised board , the panel type model is KD101N70-40NV-A002, this panel has Support in Linux or Not ?

759 Views
ganeshmc
Contributor I

I am Using iMX6Q - sabresd cusomised board to boot android and linux , the panel type model  is  KD101N70-40NV-A002, 10.1", TFT LCD , IC:0TD7107B-C/OTD9800A-C8 driver . It works fine in android but fails to get display when I boot in Linux. We set the resolution as 1280x800 in dtb file .. we are to boot the linux upto command mode .. Unable to get the graphical display in linux ( debian based OS ). Is the panel K&D- WXGA has support in linux or not..

Tags (2)
0 Kudos
1 Reply

339 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

this depends on used bsp, nxp linux documentation describes supported

panels in Release Notes, found in linux doc package

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS 

other vendors may support more panels, for example on below link

Configuring i.MX6 boards for different screens - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos