Windows 10 + Codewarrior ssh + LA1575?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 + Codewarrior ssh + LA1575?

572 Views
RandyKrakora
NXP Employee
NXP Employee

Trying to run programs via codewarrior using ssh to LA1575.

I'm getting this error:

win10-CW-ssh-error.png

Any ideas what could be wrong? Seems to build fine, I can use CW tap and connect to the target and reflash, etc. Also - I can ssh from putty on the same PC to the target.

Version: 11.3.0
Build Id: 180126

Regards,

Randy Krakora

Tags (1)
0 Kudos
1 Reply

390 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Randy Krakora,

Are you debugging Linux application project?

If yes, please refer to the section "8.2.2.2 Updating remote connection" in C:\Freescale\CW4NET_v2018.01\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to configure the debug connection property.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos