access pcie switch regs which locate high address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

access pcie switch regs which locate high address

719 Views
skwang
Contributor I

Hi  My platform os linux  work on IMX6, FPGA via switch connect to IMX RC,I use linux tools of lspci/setpci to access switch regs,  but when addresses more then 0x1000,something wrong, lspci/setpci can't work,  anybody help me

switch regs initial by EEROM,but I  can't burn EEROM everytime, so I need strong tools like lspci to  access more then 0x1000 address;  Sincere thanks

Labels (2)
Tags (1)
0 Kudos
1 Reply

557 Views
igorpadykov
NXP Employee
NXP Employee

Hi sk

please look at some limitations described on

PCIe BAR length limit 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos