Hi all
I have a question about I.MX6ULL DDR3 Script Aid which is download from below.
https://community.nxp.com/docs/DOC-333791
My customer choose MT41K256M16TW-107 IT:P due to the device availability.
Q1.
I know that i.MX6ULL only support 800MB/s.
When the speed grade of DDR3L connected to IMX 6ULL is DDR 3-1866, can we select DDR3-1866 in "Memory Type” field of the Register configuration sheet ?
Q2.
In above case, can we follow the parameter of speed grade for 107 ?
Ko-hey
Solved! Go to Solution.
Hi Ko-hey
1. customer can sellect 1600 grade for 1866 grade design (seems
DDR3-1600 option is max. in DDR3 Script Aid)
2. should be followed 1600 parameters and Table 1 footnote1 states:
107- Backward compatible to 1600.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
1. customer can sellect 1600 grade for 1866 grade design (seems
DDR3-1600 option is max. in DDR3 Script Aid)
2. should be followed 1600 parameters and Table 1 footnote1 states:
107- Backward compatible to 1600.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------