AnsweredAssumed Answered

What addresses map to SRAM in the K64 sub-family?

Question asked by Brian Silverman on Feb 5, 2018
Latest reply on Feb 7, 2018 by Hui_Ma

"3.5.3.1 SRAM sizes" in the K64 Sub-Family Reference Manual (K64P144M120SF5RM Rev. 3, July 2017) lists the SRAM_U size for some parts (MK64FX512VMD12 for example) as 192K and SRAM_L as 64K, but then has a 192K address range. Is the address range wrong?

 

Note that the total SRAM is also listed as 256K in that table and other places, so I suspect the address range is the piece of information that's wrong, but it's hard to tell what's correct for sure.

Outcomes