AnsweredAssumed Answered

Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?

Question asked by Randy Fields on Feb 1, 2018
Latest reply on Mar 2, 2018 by xiangjun.rong

I have used KMS to identify my motor parameters and create a simple motion plan using the USER_RUN_PLAN command that I successfully downloaded and ran on my eval platform.  I now would like to create an application using the USER_RUN_SPEED command and cannot get the motor to turn.  Is there an example of creating a project for applications other than running a motion plan?

Outcomes