is possible to migrate a KDS project to Mcuxpresso?
Hello
There is a tutorial aobut import project from KDS to MCUXpresso IDE:
MCUXpresso IDE: Importing Kinetis Design Studio Projects | MCU on Eclipse
While I think the easy way it create a new project on MCUXpresso ,
and then copy in the custom source code and other modifications. Minimal code re-write should be required since the drivers are the same. They are also both Eclipse/GCC based IDEs so predefines should be straight forward to port over.
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------