AnsweredAssumed Answered

Need to interface MT9P031 image sensor with imx6 dual scm, the output format of the camera is 12-bit Bayer RGB format, although the parallel camera port of the processor supports the Bayer RGB data, but it only supports 8-bit, 9-10 bit or 16 bit patterns.

Question asked by Ashvin Geete on Jan 31, 2018
Latest reply on Jan 31, 2018 by igorpadykov

Need to interface MT9P031 image sensor with imx6 dual scm, the output format of the camera is 12-bit Bayer RGB format, although the parallel camera port of the processor supports the Bayer RGB data, but it only supports 8-bit, 9-10 bit or 16 bit patterns. can we use 16 bit for 12 bit data with MSBs as 0

Outcomes