Hello BP,
Using a 32.768kHz crystal, it would appear to be feasible provided you set up the ICS for a DCO frequency of 59.77MHz (see Table 11.7 of the reference manual), and a BDIV setting to provide a bus frequency of 14.9422 MHz. If my calculations are correct, it should then be possible to provide a baud rate of 466,944 (BR = 2). This is 1.3 percent higher than the required baud rate, but should normally be satisfactory.
Since you only need to send characters at the high baud rate, an alternative approach might be to bit bang the SCI send process, and once the lower baud rate was selected, to then enable the SCI module for further communications. This might apply if you could not use the above ICS setting for any reason.
Regards,
Mac