Yocto S32V Kernel Panic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto S32V Kernel Panic

1,727 Views
hennadiyyatskov
Contributor I

We are currently building the BSP 15 for the S32V. The Yocto build is successfull and we can boot from the generated image. However during boot, we get a kernel panic, the init script simply fails with an error (-2).

I've attached the latest bootlog, were I tried to start init directly using init=/sbin/init.sysvinit, sadly the result is the same as for init=/sbin/init

Labels (1)
0 Kudos
Reply
1 Reply

1,375 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Hennadiy,

Did you used correct components from the Yocto build? I mean u-boot, dtb file, rootfs, image.

Please use the latest BSP available (now v16.1) and try again.

Thanks,

Kushal

0 Kudos
Reply