ETPU engine control CRANK problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETPU engine control CRANK problem

765 Views
haizhougeng
NXP Employee
NXP Employee

Hi

 I am new to eTPU/eTPU2 usage.

I have followed both AN3769SW and AN47908SW to set up my project on MPC5777C EVB. Toothgen function works well. CRANK and CAM signal can be observed by oscilloscope.  But the CRANK function don't work well. I find the state of CRANK always stay in Initial State, FS_ETPU_CRANK_SEEK (AN47908SW )or FS_ETPU_CRANK_BLANK_TIME(AN3769SW).

I have tried many types of configuration but never let the state of CRANK change. I think it shouldn't be so hard, but I don't know waht can I do next.

Today I try the same code on MPC5746R board. It works well. Is there some difference between MPC5746R and MPC5777C when config ETPU?

 

Thanks in advance.

Best regards

etpu2   #engine control etpu mpc5777c‌

0 Kudos
1 Reply

539 Views
haizhougeng
NXP Employee
NXP Employee

OK. I have fixed this issue. For MPC5777C, I have to config IGF if I use EPTUx as input. And if I follow AN3769, I muse config EPTU0 as crank channel.

0 Kudos