Hi,
I am using IMX.7 in combination with Yocto Project.
I follow steps mentioned in
it took 6 hours on ubuntu to compile bsp and built sd card image.
but didn't understand where to add/edit source code lets say for UART/PCIE etc.
Hello,
Please refer to "i.MX_BSP_Porting_Guide.pdf".
In particular - use Chapter 2 (Porting Kernel) and Chapter 3 (Porting U-Boot).
https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------