i.MX6SoloX support 12MPx camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SoloX support 12MPx camera

385 Views
stefankolody
Contributor I

Can  i.MX6SoloX support 12MPx camera sensor and it's full resolution throughput without any slowdown all the way to the memory?

Labels (1)
0 Kudos
1 Reply

315 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

For the 12MPx camera sensor, the data output by camera is RAW data, in the i.MX6SX there is no ISP moudule, so it can not work on the i.MX6SX.

In the i.MX6 design, need your camera with the ISP function. The mux clock of CSI is 264MHz, your camera resolution work clock should below the mux value. So, the1080P @30 can work.

Have a nice day

Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos